Top 5 Circuit Breakers
This article will focus on the very best circuit breakers that are available right now. Each of these circuit breakers can be found using oemsecrets.com with the help of our wide range of distributors that supply these products. The article will highlight these circuit breakers based on several important elements, such as:
- What each of these circuit breakers looks like
- Key features that differentiate each of these items from one another
- Performance levels for all of these circuit breakers
- Positives and negatives for all of these products
- The general customer response to these items so far
What is a Circuit Breaker?
A circuit breaker is a device that uses electricity to protect the main circuit from any damage that could come from an overcurrent or a short circuit. The idea is to reduce the flow of an electrical current in order to protect the key elements, thus also reducing any possibility of a fire. Now, circuit breakers are used in so many ways across the home, and this applies as well to major offices, particularly those that rely on electricity for a business to function on a daily basis.

Weidmuller – 6720005302
Square D By Schneider Electric – HJL36030M71
Phoenix Contact - 2905743
Eaton Cutler Hammer – FDE308032
ETA Power Europe – REX12-TA1-107-DC24V-1A