5 of the Best Single Board Computers of 2022
Single Board Computers are available through oemsecrets.com from leading suppliers and manufacturers like Adafruit, Beagleboard, Intel, Raspberry Pi, Seeed Studio & more.
In this blog we will be shining the light on a few SBCs and highlighting various aspect of the product based on our research which will include:
- We’ll show you what the product is like physically
- We’ll explain what sets this product apart from its competition
- We’ll highlight any comparable products
- We’ll highlight pro and cons we found
- We’ll highlight what people think of the product
We will be keeping you updated as new SBCs gets released, so without further ado, let us go straight and discuss the Best Single Board Computer of 2021!
What is a Single Board Computer (SBC)?
1. Raspberry Pi 4
Raspberry Pi is now a household name and has the biggest support and development community which is why this product is the best for anyone new to a single board computer.
At the time of writing RS components had the best price at £58.40 for the Pi 4 8GB model B.
What's special about this Raspberry Pi 4?
The price is affordable, and we know it can run some high performance tasks like video scaling because of features like its powerful graphics processing unit (GPU).

Features:
CPU: Broadcom BCM2711,
Quad core Cortex-A72
(ARM v8) 64-bit SoC 1.5GHz
GPU: Broadcom VideoCore VI
Memory: LPDDR4 SDRAM
Connectivity: Bluetooth 5.0,
Dualband 2.4 & 5GHz wireless,
Gigabit ethernet, PoE
2. Rock Pi 4 Model C
At the time of writing Distrelec had the best price at £58.40 for the Rock Pi 4 model C.
What's special about this Rock Pi 4 Model C?
A few things we thought they could improve is the level of support as this could be a problem since they haven’t got a bigger community base like Raspberry Pi do. affordable, and we know it can run some high-performance tasks like video scaling because of features like its powerful graphics processing unit (GPU).
Features:
CPU: Rockchip RK3399,
Quad core Cortex-A53 (ARM v8)
64-bit 1.4 GHz
GPU: Mali T860MP4
Memory: LPDDR4-3200
Connectivity: Bluetooth 5.0,
Dualband 2.4 & 5GHz wireless,
Gigabit ethernet
3. Asus Tinker Board 2S
At the time of we didn’t have this listed on our website but we’’ get you a link as to where you can get one of this at the best price.
What's special about this Asus Tinker Board 2S?
What we noticed as well is, it comes with an RTC header and the manufacture also notes that it comes with protection against electrostatic discharge and overvoltage.
Features:
CPU: Rockchip RK3399 ARM
64-bit architecture, 1.8 GHz
GPU: Mali T860 MP4
Memory: 2 GB LPDDR4
Connectivity: Bluetooth 5.0,
Dualband 2.4 & 5GHz wireless,
Gigabit ethernet, BLE
4. Arduino Mega 2560
It features more memory and pins to be precise a 54 digital input/output pins which gives you better equipment performance and according to the datasheet 15 pins can be used as PWM outputs, 16 analog inputs, and 4 UART hardware serial ports.
At the time of writing Mouser had a few in stock with the best price at £28.99 for the Arduino Mega 2560.
What's special about this Arduino Mega 2560?
The price is affordable, it comes with a USB connection as well as a handy reset button.
Features:
CPU: ATmega2560, with a
RISC, 8-bit architecture, 16MHz
GPU: n/a
Memory: 8 KB SRAM, 4 KB EEPROM
Connectivity: None
5. PocketBeagle
It has a sleek design and most importantly it doesn’t cost much and at the time of writing Farnell electronics & element14 had the best price at £28.50 for the PocketBeagle (BB-POCKET).
What's special about this PocketBeagle?
Beagle products are designed to accommodate open-source and this PocketBeagle allows for imagination and greater learning potential. It also has 72 expansion pin headers and 44 digital I/Os for expansion and better interfacing.
Features:
CPU: Octavo Systems
OSD3358-SM, ARM Cortex-A8 CPU, 1GHz
GPU: PowerVR SGX530
Memory: 512 MB DDR3
Connectivity: None
Summary
There are dozens of other SBCs, but we have only highlighted a few you can quickly get your hands on even with parts shortages. So, which one should you choose? This is entirely dependent on your project.
Send us some feedback and we’ll keep adding onto this list.