Today we are shining the spotlight on the STM32F405RGT6 microcontroller. This is available right now from OEM Secrets, with STMicroelectronics as its manufacturer and Farnell as the distributor. So, allow us to discuss why this is a microcontroller that you need to purchase today.

STM32F405RGT6 Microcontroller by STMicroelectronics
STM32F405RGT6 Microcontroller

Explanation

This product is a primary example of the power that lies within a microcontroller. Every machine that we use relies on a source of power that ensures the delivery of all its functions. That could be anything from setting up a timer to heating up a surface to powering up a motor. In all of those examples, the real work happens due to the presence of a microcontroller. This powerful yet miniscule kit acts as the mechanical nerve centre for the appliance. Without it, the machine cannot function. And therefore its presence is vital, but you also need to know that the machine is performing at full capacity. And you can be sure to receive this by using this particular product as the microcontroller for your office and home machinery.

 

STM32F405RGT6 Technical Specifications

The STM32F405RGT6 serves as a 32-bit microcontroller which forms part of a larger STM32 group of microcontroller products. This has ARM Cortex-4 architecture, along with 1MB of memory and 196kb of RAM. Providing a powerful CPU speed of 168 MHZ with 64 pins, this product offers 6 PWM Channels within its technical set-up. In addition, the product’s supply voltage goes between a minimum of 1.8V and a maximum of 3.6V. Not to mention the item’s CAN I2C SPI UART USART USB embedded interface. Following on from this, this possesses fourteen timers, a strong number in line with its competitors. And to round things off, this popular microcontroller has a temperature range going from -40°C right up to 85°C and beyond.

Other Notes

The product comes with an instruction manual for installation or a STM32F405RGT6 datasheet with all the important technical notes for this product. Note that while appliances come in all shapes and sizes, their internal makeup often shares numerous visual traits. As a result, if you learn to install the microcontroller into one machine, you should quickly understand how that applies to other machines. And this is ideal if you’re purchasing a batch of these products. That’s because a quick installation of each of them means you having several high-performance appliances all at the same time. Not forgetting how a microcontroller could bring new life to a machine that a customer may previously assume is broken down.

Why You Need The STM32F405RGT6

As the world relies more on technology, the machines themselves have to be up to standard. And therefore it can be problematic if age, poor set-up or simply a lack of logical design renders an appliance as unusable. Alternatively, you may be using the machine, but it may be offering very little performance and, consequently, very little satisfaction. But that’s why a microcontroller such as this becomes crucial, because it allows you to receive value for money on any appliance you have. And when it comes to a standard-bearer like the STM32F405RGT6, the upgrade in quality and output is immediately noticeable. And you only need to purchase one per machine because you’re going to get many years of top-notch productivity from this microcontroller.

Contact Us

The normal asking price for the STM32F405RGT6 microcontroller is £11.89 per break. Now, to take a closer look at this product, please visit https://www.oemsecrets.com/details/stm32f405rgt6. However, you can also speak to our member of our team by emailing info@oemsecrets.com.

Author: Mark Armstrong
Published: August 12, 2021