In this article, we are going to discuss the LIS2DH12TR accelerometer electronic component. This product is manufactured by STMicroelectronics, and it is available to buy right now on oemsecrets from a variety of authorised distributors. These include the likes of Mouser Electronics UK, Newark Electronics and RS Components UK. But what makes the LIS2DH12TR stand out amongst the competition? We will now go into detail on this very subject.

LIS2DH12TR accelerometer

Explanation

The LIS2DH12TR accelerometer is a digital output motion sensor. This means that the product offers a combination of ultra-low power and high performance, which is just the right balance that users need. Furthermore, this accelerometer is capable of measuring accelerations with output data rates ranging from 1 Hz to 5.3 Hz. The self-test capability allows the user to check the sensor’s functionality in the final application. Keep in mind that this accelerometer sits within the internal framework of so many things that we use in daily life. This includes everything from videogames consoles and virtual reality (VR) headsets to pedometers and digital watches. Indeed, the accelerometer is central to the operation of many devices. And the LIS2DH12TR is highly recommended by industry experts as being one of the absolute best accelerometers out there.

Technical Specifications of the LIS2DH12 Accelerometer

The LIS2DH12 is an ultra-low-power high- performance three-axis linear accelerometer. It belongs to the “femto” family and provides digital I2C/SPI serial interface standard output. It has a wide supply voltage ranging from 1.71 V to 3.6 V. Note that it is compatible with both independent IO supply and supply voltage. And it has two independent programmable interrupt generators when it comes to offering free fall and motion detection. Its temperature sensor is a further reason to invest in this particular accelerometer.

Other Notes

Alongside these technical points, the LIS2DH12 is easy to install and operate by following the instructions that are included within the package when you place an order for this item. It is an innovative and intelligent product that enhances gaming (and other) experiences, and of course it also has the aforementioned self-testing capability that allows the user to ensure that the product is functional upon its final application. All of which makes it even more impressive that this accelerometer is able to perform its tasks to an extremely high operational standard. 

Why You Need The LIS2DH12 Accelerometer 

As much as we enjoy gaming, we want such experiences to be elevated and enhanced as much as possible. And that is exactly what the LIS2DH12 accelerometer does, hence the integration of the phrase “accelerate”. The product is small and thin, and it is able to operate over an extended temperature range, meaning you don’t need to compromise when it comes to the activities you enjoy. If your usage requires the highest performance possible, we suggest that the best option on the market today is the LIS2DH12 accelerometer.

Pricing And Availability 

The lowest break price for the LIS2DH12 accelerometer is £1.04 courtesy of RS Components UK, which is in stock and available to buy right now from oemsecrets. To find out more about the product and to compare prices and availability, please visit https://www.oemsecrets.com/details/lis2dh12tr.

Author: Mark Armstrong
Published: August 12, 2021