Join The Tool Rebellion with Wera Hand Tools

Using high-quality hand tools makes tasks such as test equipment disassembly or equipment repair much more productive. Wera, based in Wuppertal, is popular among both electrical engineers and handymen. This article introduces a few interesting product families.
Wera's history has been driven by innovation. Technologies for products such as Zyklop or Joker were not only the first to market, but also, in many cases, revolutionized the way hand tools work.
Eternally focused on usability, many of Wera's tools are color-coded. This simplifies finding the right component and dramatically accelerates workstation cleanup after an assembly job.
Wera Green or Wera Red?
Wera's tools are often used by electricians working in actively powered systems. For this, VDE certification---the acronym stands for Verband der Elektrotechnik, which means the association of electrical engineering---is of paramount importance both for code compliance and security. The red-handled screwdrivers---an example set is the 05006618001 shown below---undergo these certifications.

If the tools are used only outside of live systems, VDE certification is not necessary. In this case, the green tools---an example is 05051060001---can be used.
Compact Storing via the Tool-Check System
Hand tools tend to get lost or messy when not stored in storage containers. With the Tool-Check system, Wera provides a new way ideally suited for home office and mobile use. For example, let us look at 05049002001, as shown in the figure below.

Thanks to each bit and its associated tooling having a defined space, missing tools and bits can be easily found and purchased individually. Furthermore, the Tool-Check system can be snapped together to create a bar of tools. Using the 05049004001 adapter provides a 90° bend, making the tool stand ideal for filling otherwise-unused space on test benches.
Wera also supports engineering on the go with a variety of portable kits that include a carrying case. One interesting example is 05004187001, which is suited to cyclists.
Conclusion
Investing in high-quality hand tools is always a good idea. Wera is a brand that stands out for both innovative ideas and traditional, high-quality workmanship. In short, it is a brand that always deserves consideration when planning tool purchases.