On this blog, we are going to describe the main benefits from both a performance and technical standpoint of the DS1822+ IC temperature sensor. This is a part that is manufactured by Maxim Integrated. And you can buy this item today through oemsecrets from such distributors as Mouser Electronics UK, RS Electronics UK and Future Electronics. With all that being said, we will now break down the specific details about this high spec IC temperature sensor product.

 

Explanation 

The DS1822+IC temperature sensor acts as a digital thermometer which simplifies distributed temperature sensing with multi-drop capability. Only one port pin is required for its internal communications to perform as necessary. A digital thermometer is hugely important to the functionality of thermostatic controls, industrial systems, consumer products, thermometers or any thermally sensitive system. And so the DS1822+IC sets the industry standard when it comes to first-class digital thermometer performance, quality and longevity.

 

DS1822+ Technical Specifications

The DS1822+ has a unique 1-wire interface, which requires only one port pin. So, it can be powered from data line, and it also boasts a power supply range of 3.0V to 5.0V. In addition, the product has a reduced component count with an integrated temperature sensor and interface, meaning it does not require any external components. It also measures temperatures from -55°C to +125°C (-67°F to +257°F), boasts a ±2.0°C Accuracy from -10°C to +85°C, and it converts the temperature to 12-Bit Digital Word in 750ms (max).

Other Technical Notes

As well as the various features addressed above, the DS1822+ is a fantastic product as the thermoment resolution is user selectable from 9 to 12 bits. And the upshot of this is that the user is able to be in control whenever the item is being used. The product is easy to use and extremely accessible, making it an ideal and inexpensive investment for everyday use should that product be of interest to you. 

Why You Need The DS1822+

The DS1822+ by maxim integrated is one of the leading digital thermometer parts that you will find on the market. After all, there are plenty of digital thermometers available from a wide variety of manufacturers. But how many of them manage to bring together everything that you need from a performance and functionality standpoint to ensure a top-level total package on the whole? Not many. But the DS1822+ is one of those that absolutely can. And it’s all at an affordable price, which adds value for the user when bought in bulk. So, make the most of this chance to own the very best digital thermometer that is available for you to purchase today. 

Pricing And Availability

The smallest break price that you can find right now for the DS1822+ IC temperature sensor is £2.13. And so you can buy it as soon as you finish reading this article from oemsecrets. But if you need further information before you commit to making a purchase, then we advise that you head on over to https://www.oemsecrets.com/details/ds1822.