ATxmega32A4U-MH by Microchip
ATXMEGA32A4U-MH microchip

ATXMEGA32A4U-MH microchip 

The ATXMEGA32A4U-MH is an 8-bit AVR microchip that has been developed by Microchip Technology. It has proven to be a very popular and highly effective item. This chip belongs to the Atmel AVR XMEGA AU family of low-power, high-performance, and peripheral-rich CMOS 8/16-bit microcontrollers which is based on the AVR enhanced RISC architecture. 


In this article, we focus on five core benefits of the ATXMEGA32A4U-MH to explain why it's one of the market leaders for such products.

1. Low power, high performance

A first-class microchip product uses minimal power for maximum efficiency. That's what the PRODUCT does by offering 4KB internal SRAM and a 4KB boot section while also working with the same efficiency as a USB 2.0 full speed (12Mbps) drive, as well as being low speed (1.5Mbps) device compliant.

What makes this special?

This is important because, by operating with low power, the microchip doesn't compromise the overall power of the product that it is used alongside. It also ensures a longer lifespan for the microchip itself. And all while delivering the top performance levels that customers would expect and deserve.

2. Versatile uses

There are so many types of products for the ATXMEGA32A4U-MH to be used alongside. This includes industrial machinery, climate control functions, motors, handheld battery devices, power tools and major home appliances. As a microcontroller unit, it's gaining more use in other verticals including medical, optical technology as well as factory automation.

What makes this special?

The more ways that you can use a product, the greater value it has. What's more, by being able to use the same type of microchip in so many ways, there will be a consistently high level of performance across the board. This is particularly important for larger companies that require a great number of microchips across their machinery.

3. Multiple digital timers

The ATXMEGA32A4U-MH doesn't just have one 16-Bit digital timer; it has five. Note that digital timers contain a clock and enable signals that allow for internal clocks to be counted, as well as offering external pin signals to other machinery.

What makes this special?

It's unusual for a microchip to have so many digital timers. And considering the various types of appliances that this microchip can work alongside, the fact that this item has five 16-bit digital timers is a huge boost for those using the microchip in abundance.

4. Self-programmable flash

The ATXMEGA32A4U-MH has 32KB of in-system self-programmable flash. This means that the microchip is capable of updating its own flash while it's operating. This also allows for ongoing code updates.

What makes this special?

This is a major benefit because it saves time, effort, and money. Otherwise, the microchip would have to be reprogrammed and possibly replaced. Therefore, the self-programmable flash is hugely significant.

5. 32 endpoints

The ATXMEGA32A4U-MH has 32 endpoints that allow for full configuration flexibility. This allows for a high level of data to be sent and transferred via the microchip.

What makes this special?

This makes for an intelligent and versatile microchip that provides many different endpoints where data can be transferred. This also means data can be transferred faster and more effectively due to the many options available.

Pricing And Availability of  ATXMEGA32A4U-MH

The smallest break price that you can find on oemsecrets right now for the ATXMEGA32A4U-MH microchip is £2.62 (correct at time of publication) thanks to Arrow Electronics. If you want further information about this Microchip Technology product or a quote from one of the listed authorised distributors (RS components, Mouser,  Avnet, Future, Farnell, etc.), you can visit https://www.oemsecrets.com/details/atxmega32a4u-mh and compare inventory and pricing, and save your business money and time.

Author: Mark Armstrong
Published: December 6, 2021